MITSUBISHI ELECTRIC Changes for the Better

MELSEC MX Controller MX-R model

The MELSEC MX Controller is a series of controllers that integrates three types of control, sequence, motion, and network. The MELSEC MX-R diversified and sophisticated system can be constructed by using the MX-R models with the MELSEC iQ-R Series modules. 

One controller for all your control needs

Decades of expertise in programmable controller technology have been combined into a single controller. By integrating sequence control, motion control, and network control on the MELSEC MX Controller platform, faster and more accurate control is achieved. We will continue to add functionality to this platform, making it adaptable to a wide range of applications.

Equipped with a high-performance multi-core MPU as standard, enabling high-speed control

All functions of sequence, motion, and network are integrated. The motion control performance is about 10 times*1 higher than existing products of Mitsubishi Electric, achieving high-speed and high-accuracy motion control.

*1:Comparison with the MELSEC iQ-R Series (64-axis control)
*2:Device stations supporting connections to 253 stations will be available in the future. For details, refer to the Technical Bulletin (FA-A-0451).
*3:When the motion operation cycle setting is 1.5 ms

Further details of the MX-R model

The MELSEC MX Controller (MX-R model) is mounted on the MELSEC iQ-R Series main base unit and can be used in combination with the products listed in the latest catalog 

System configuration example - MX-R model

*1: Future support
*2: The multi-axis servo amplifier can control multiple axes with one station occupied.
*3: Device stations supporting connections to 253 stations will be available in the future. For details, refer to the Technical Bulletin (FA-A-0451).
*4: Only the servo can execute motion control.