FOR IMMEDIATE RELEASE No. 3173
- Highly User-friendly Interface Induces Touch -
TOKYO, February 14, 2018 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that together with a school for the visually impaired it has designed an experimental remote-control interface that enables people to easily operate equipment by using their sense of touch to recognize the intuitive shapes and movements of various controls.
The experimental remote-control interface for air conditioners was developed as a case study with the cooperation of teachers and students at a school for the visually impaired. The same principles of matching heights, shapes, etc. that the students learn at the school were adopted in developing the new interface. The unique interface uses distinctive shapes, positions and movements to signify the air conditioner's different modes and the status and operation of each function, enabling visually impaired people to easily confirm and adjust settings.
Note that the releases are accurate at the time of publication but may be subject to change without notice.